Can the Sepam series 80 voltage inputs be connected directly to a 415 V 4-wire 3-phase LV system (without the use of Voltage transformers)?

The continuous thermal withstand of the Sepam series 80 voltage inputs is 240V AC, which means that it is not possible to connect the Sepam directly to the network. Furthermore, the Sepam setting tool (SFT2841) does not allow such voltage values to be entered.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166655 V2.0, Originally authored by LaVI on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 80

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: