What is the maximum number of digital inputs the Sepam series 20 can have?

Goals and Symptoms

What is the maximum number of digital inputs the Sepam series 20 can have?

Causes and Fixes

10. It is possible to add a MES114 card which has 10 digital inputs and 4 digital outputs.

Original article#3641

Re-published to revised security level: 17 June 2008 by DRM

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL185704 V2.0, Originally authored by KBAdPM on 06/29/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 20

Schneider Electric Việt Nam