Why is the CB status of Sepam Series 40 displayed with ‘?’ mark in PowerLogic SCADA?

If you have a problem as per below, you need to check 2 things.

a. The hard-wired signals from the CB which are for CB On/Off status must be connected to Sepam 40 following the default IO setting. (Please take a Sepam 40 manual for more details.)

b. Device closed tag must be added into your project.

You can find this tag under Sepam Series 40 with default IO device type -> Miscellaneous -> Real Time Tags in PowerLogic SCADA Profile Editor.

Check also last Updated information from our PowerLogic L3 Team

Key words and phrases:

question mark, meaning, signification, signify, mean, what

AEBL3

Original Author: YJ

Public

All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200477 V2.0, Originally authored by KBAdPM on 11/11/2009, Last Edited by DaMi on 01/22/2010
Related ranges: Sepam series 40, PowerLogic SCADA 7.1

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: