Video: What is Modbus Tester and how do I use it?

Issue
Need a simple tool that can read Modbus registers.

Product Line
Modbus Tester

Cause
Diagnosing communications or verifying values.

Resolution
Modbus Tester is a simple register reading/writing program. The below screen shot details each commonly used value block, and the video below shows how to read and write to registers. Note: Modbus Tester is hardcoded to port 502.

Modbus Tester



Attached is a copy of the program.

Schneider Electric Việt Nam

Phần đính kèm
Tester.exe [204 KB]