MiCOM S1 Studio Error: Data model file is not installed

Issue
Error message: "Data model file is not installed"

Product Line
MiCOM relays

Environment
MiCOM S1 Studio

Cause
This error will populate in MiCOM S1 Studio if one is attempting to connect to a MiCOM relay without the data model being installed.

Resolution
Refer to FA221295 for detailed instructions on how to add the data models.
The latest version of Easergy Studio (MiCOM S1 Studio) can be found here: https://www.se.com/ww/en/product-range-download/61035-micom-s1-studio


Legacy KB System (APS) Data: RESL210416 V1.0, Originally authored by DaFr on 01/24/2013, Last Edited by DaFr on 01/24/2013
Related ranges: MiCOM S1 Studio

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: