What are the ambient temperature requirements for power transformers to meet IEEE C57.12.00-2000?

According to the IEEE C57.12.00-2000 standard, power transformers are rated at a maximum ambient temperature of 40 degrees Celsius with the average ambient temperature not to exceed 30 degrees Celsius in any 24-hour period.

Schneider Electric Việt Nam