Why doesn't the program allow you to choose to upgrade to TXBT-F?

Facts and Changes

xbtl1000
XBTF
TXBTF
conversion
Application

Causes and Fixes

The second program has a "FORM" page. If you delete the "FORM" page then it is possible to see and choose an TXBT product.
The TXBT has an hard disk working with Windows OS.
In this case, you don't really need forms, because it's possible to find other solutions, such as "screen hardcopy", macro with Word.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: