Tìm các câu hỏi thường gặp
How do we include the Editor project (.VDZ backup project file) in the HMI with Vijeo Designer V6.2?
Issue
How do we include the Editor project (.VDZ backup project file) in the HMI with Vijeo Designer V6.2?
Product Line
Vijeo Designer v6.2
Environment
Magelis / Harmony HMI Configuration software in Windows
Resolution
Under the download section, tick the Include Editor Project setting checkbox to activate it. By default this option is unticked and deactivated.
Go to Data location and set the Data Files / Forms Drive to where you want the .VDZ backup file to be stored. You can select between Main (Internal memory), Secondary (CF or SD Card depending on model) and Optional (USB memory stick) drives depending on the HMI model.
If you choose Main, to allow Vijeo Designer Data Manager to access the HMI in the future:
1. In the Project Navigator, select the Environment->Security node.
2. In the Property Inspector window, next to Download Security, choose either "Anonymous", or "Use Security"