Can I connect a USB barcode scanner and a USB printer to a HMISTU655/855?

Issue:
connecting a USB barcode scanner and a USB printer to a HMISTU655/855?


Product Line:
HMISTU655/855


Resolution:
Yes, you can connect both USB barcode scanner and printer to the HMISTU655/855 but the target only have
one USB port. You will need to use a USB hub.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: