What is the minimum Vijeo Designer version which will program the HMISTU series?
Issue:
Unable to download to my brand new HMISTU855 or HMISTU655 with Vijeo Designer

Product Line:
HMISTU Series, HMISTU655, HMISTU855, HMIS5T

Resolution:
For HMIS5T rear modules with PV:09 RL.16 SV:6.0 or greater, we must use Vijeo Designer 6.2 SP7 or greater. For any PV, RL, SV numbers that are older we can use Vijeo Designer 6.2 SP6 or older. The minimum version is Vijeo Designer 5.1 SP2.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: