How to connect the output LO1 of the ATS01

Goals and Symptoms


How to connect the output LO1 of the ATS01.

Facts and Changes

ATS01 and output LO1

Causes and Fixes

See the diagram in the attachment file.

Attachments

(Removed File URL: 162371_54B6/Example_of_diagram_to_use_the_ATS01's_LO1.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/45c7ad418107e309c125708b004a6b13/fl_block_5/0.1402?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL162371 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48

Schneider Electric Việt Nam

Phần đính kèm
Example_of_diagram_to_use_the_ATS01's_LO1.zip [27.53 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: