Tìm các câu hỏi thường gặp
Why is the status LED on my XBT-G Magelis unit orange?
Issue
Why is the status LED on my XBT-G Magelis unit orange?
Product Line
XBT-G Magelis
Environment
XBT-G Magelis
Resolution
The status LED on the XBT-G Magelis units will illuminate orange to indicate the backlight has burned out. The unit will need to have its backlight replaced. The table below lists the various Magelis XBT G terminals and their corresponding replacement backlight bulb part numbers:
XBT G Terminals | Backlight Bulb |
XBT G2120/G2130/G2220 | XBTZG12 |
XBT G4320/G4330 | XBTZG14 |
XBT G5230 | XBTZG13 |
XBT G5330 | XBTZG15 |
XBT G6330 | XBTZG16 |
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: