Tìm các câu hỏi thường gặp
Can the 6000-021 Cybercalc software be run on Pentium based PCs?
Issue
Can the 6000-021 Cybercalc software be run on Pentium based PCs?
Product line
Cybercalc
Environment
6000-021
Resolution
The 6000-021 Cybercalc software is not qualified for usage on Pentium based PCs, however it has been used previously with success. You may need to run SLODOS, CPUKILLER, or other freeware to slow the PC down.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: