Tìm các câu hỏi thường gặp
What causes a "Runtime Error 372 - Failed to load control 'LFile' from SKCL.dll. Your version of SKCL.dll may be outdated"?
This error usually occurs when authorizing Concept, Proworx or Control Expert 14 (Unity Pro software. The SKCL.dll must reside in the \windows\system32 or \winnt\system32 folder. If it currently resides in this folder, you may need to register the .DLL.
To do this, bring up a DOS shell and type:
c:\> regsvr32 skcl.dll
You should then be able to launch the Authorization utility.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: