TCSESM ConneXium Switches and FW version 4.1

Issue

Users of ConneXium TCSESM switches may experience a failure of the Web pages to function properly.

Product Line

ConneXium - Switch

Environment

TCSESM v4.1

Resolution

On your PC select Start->Settings->Control Panel->Java. This will open the Java Control Panel. Select the Advanced tab. Expand the Java Plug-in Branch and de-select the box (Enable the next-generation Java Plug-in). Click the OK button.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: