Tìm các câu hỏi thường gặp
How do I setup Vijeo Citect V7.0 for redundant LAN?
Goals and Symptoms
The purpose of this resolution is to provide a solution for LAN redundancy with Vijeo Citect V7.0
Causes and Fixes
This requires two NIC cards in the Vijeo Citect server PC. It is recommended to run the ethernet cable to a different path (conduit) to another ethernet switch. So that in the event of a link or ethernet switch failure, the other path may still provide data to the Vijeo Citect I/O Server.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: