Tìm các câu hỏi thường gặp
Within the catalogs in the characteristics section for the RPF relays, it mentions that for the Rated operational current in utilisation categories AC...
Goals and Symptoms
Within the catalogs in the characteristics section for the RPF relays, it mentions that for the Rated operational current in utilisation categories AC-1 and DC-1: Conforming to IEC N/O=30A N/C=3A Conforming to UL 30A. Why is so big the difference between N/O and N/C ratings in IEC?
Causes and Fixes
The NO contact is dedicated to switch power loads.
The NC contact is dedicated for low power control (PLC, pilot light...)
Legacy KB System (APS) Data: RESL200159 V1.0, Originally authored by LaBe on 10/02/2009, Last Edited by LaBe on 10/02/2009
Related ranges: Zelio Relay
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: