Tìm các câu hỏi thường gặp
What does a blinking red power light on the XBTGT Magelis series indicate?
A blinking red led indicator lamp on the XBTGT range indicates either a system fault, or a power fault. Please refer to the electrical specifications below:
Electrical
[Us] rated supply voltage | 24 V DC |
Inrush current | <=30 A |
Power consumption | 42 W |
Supply | External source |
Supply voltage limits | 19.2 V-28.8 V |
If power specs are correct please contact Technical Support at 888-266-8705, Option #1.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: