What is the recommended number of wires and AWG size for connection to a BMXFTB2820 or BMXFTB2800 ?

Issue
Need to purchase wire and need to know acceptable sizes.

Product Line
Modicon X80 IO

Resolution
The recommendation is one wire between 16 to 24 AWG.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: