Product line
Energy Meters (EMB and EME series)
Environment
Energy Meter Installation
Resolution
The energy meters have been tested and verified functionality with the CTs mounted up to a maximum distance of 300 feet from the meter using 18 AWG twisted leads with 600V insulation (UL 1015 or equivalent).