Tìm các câu hỏi thường gặp
ION7300 Series Obsolescence (obsolete) End of Commercialization
Issue
ION 73xx series Obsolescence (obsolete) End of Commercialization
Product Line
ION7300
ION7330
ION7350
Cause
Customer wants to order the ION73xx series meter but is it available for sale?
Environment
End of commercialization and recommended replacement
Resolution
The end of commercialization date is January 31, 2016, with a last time buy date is January 8, 2016, subject to product availability.
NOTE: The direct replacement for the ION 7330 and ION 7350 meters is the PM8000 series meter (Part Number: METSEPM8240).
The ION73xx will continue to be repaired until December 2017 as parts allow.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: