Tìm các câu hỏi thường gặp
Does the Modbus Cradle Communication Module (CCM) support 2 wire RS485 communications?
Issue:
User may need to connect the CCM to a 2 wire daisy chain.
Product Line:
Cradle Communication Module
Environment:
RS-485 Communications
Resolution:
The Modbus Cradle Communications Module does support 2 wire RS485 communications. The module can be configured by jumpering the IN+ and the OUT+ and the IN- and the OUT-.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: