What is the RJ11 Pinout for the 6200 TRAN Meter?

Below is the pinout for the 6200 TRAN RJ11 Connector for the Modular Display:

Pin 1: Vcc
Pin 2: GND
Pin 3: -Signal
Pin 4: +Signal
Pin 5: GND
Pin 6: Vcc




Last Revised: September 21, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188295 V1.0, Originally authored by KBAdPM on 10/04/2007, Last Edited by KBAdPM on 10/04/2007
Related ranges: ION6200

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: