Does Service Update 1 Need To Be Run Before Service Update 2 On SER Version 7.1?

No. The fixes made in Service Update 1 were rolled into Service Update 2 along with additional modifications. The user only need run Service Update 2 after the initial SER 7.1 install.


Legacy KB System (APS) Data: RESL198183 V1.0, Originally authored by AnVa on 04/01/2009, Last Edited by AnVa on 04/01/2009
Related ranges: Sequence of Events Recorder (SER)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: