The kVAR (Reactive Power) and PF (Power Factor) readings are incorrect when using Transformer Line Loss - Method 2 on the ION8600, ION7650, or ION7550.

Goals and Symptoms

After enabling the transformer line loss method 2, kW (Real Power) and kVA (Apparent Power) read correctly, however kVAR and PF are reading much lower than the uncompensated meter.

Causes and Fixes

This can happen if the incorrect values are put into setup registers %LVFe and %LVCu for method 2. These 2 parameters are mainly used in the calculation of compensated kVAR.



Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/8da474ca3e665ecbc12575cc00109a14/fl_block_5/0.1AD6?OpenElement&FieldElemFormat=gif)
Date Created: June 1, 2009
Last Revised: June 4, 2009
Public
Original Author: MC
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199084 V1.0, Originally authored by MiNe on 06/05/2009, Last Edited by MiNe on 06/05/2009
Related ranges: ION8600, ION7550/ION7650

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: