How do I add ION8650 Support in ION Enterprise 6 ?

Issue
ION 6 does not include an ION8650 driver natively, user wishes to add the native driver to the ION Enterprise system.

Product Line
ION Enterprise 6

Environment
Driver Install

Cause
ION8650 came out after ION Enterprise 6 and was not part of the software during release.

Resolution
In order to add ION8650 support in ION Enterprise 6 you will need to run the linked ION8650 device updater on the primary ION Enterprise 6 server.
You can download the device updater from the global Schneider Electric Website at the following link below

https://www.se.com/hk/en/download/document/ION8650_Device_Updater/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: