Title
Installing a new M340 CPU SD card
Issue
Installing new SD card into M340
Product Line
M340
Environment
Unity Pro, Control Expert
Resolution
Procedure:
1. Make sure new SD card is in the Unlock position.
2. Insert new SD card into M340 memory card slot and the LED will turn ON.
3. Open the Animation Table Window.
4. Add system bit %S65.
5. Turn on the Modification button.
6. Enter value 0 for %S65 and close door.
7. Start PLC
Đã phát hành cho:Schneider Electric Việt Nam