What is the maximum number of nodes allowed on one Profibus network?

The maximum number of nodes per bus for a Profibus network is 32 without repeaters.
125 nodes may be used with 3 repeaters and 4 network segments.
They can be addressed 1-126.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: