Instrument Transformers 600V Indoor type Current and Voltage

Issue
Customer is looking for datasheet for Class 4210 Voltage and Current transformers.

Product Line
Class 4210 Transformers

Cause
Customer is looking for datasheet for Class 4210 Voltage and Current transformers.

Environment
Datasheet and specification for Class 4210 Transformers.

Resolution
The datasheet for Class 4210 Transformers are attached below.

Schneider Electric Việt Nam

Phần đính kèm
Instrument Current and Voltage Transformers.pdf [4 MB]