Symptom:
Vista queries work but the same query in Webreach returns:
------------------------------------------------
Webreach error:
"Pegquery error (80040c8e)"
"ActiveX component cannot create object"
"/ion/historical/getlogs.asp line 51"
-----------------------------------------------
This is often due to Vista inheritance issues. To fix:
1) Open Vista
2) Navigate to the Top level window (all the Vista diagrams are linked to each other with Parent-Child relationships)
3) Open the Toolbox and right click on the background
4) Under the Query Server tab select Edit Link> Choose Query1 (or any custom query server)
5) Click OK and save this
After completing the above simple procedure, webreach historical data for this query should work.
Đã phát hành cho:Schneider Electric Việt Nam