What quantity does V Avg represent on the front panel display of an ION6200 in delta mode?

The ION6200 can measure V L-L Avg as well as V L-N Avg, however in delta mode, since there is no neutral, V L-N Avg is not available. What is shown on the front panel display is V L-L Avg and it is labeled V Avg. The meter's firmware is designed to display this quantity on the front panel. Having said that, V L-N Avg is available through Modbus or ION protocol with any ION software.



  • Date Created: June 13, 2008
    Last Revised: February 16, 2009
    Public
    Original Author: KG
    All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL197835 V1.0, Originally authored by KBAdPM on 02/17/2009, Last Edited by KBAdPM on 02/17/2009
Related ranges: ION6200

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: