Is there a script in Vijeo Designer that will allow me to write a new IP address of an Equipment at Runtime?

Issue:
Writing a new IP address of an Equipment at Runtime in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
Yes, you can write the IP address of an equipment via scripting. This feature was implemented in Vijeo Designer V5.0 SP1. This code will set IP Addresses for any driver, not just the Modbus driver. Below is an example script:


  • // --------------- Write some data -----------------------------------------

    // Length is given by NewIP_InputData.length

      • int [ ] NewIP_InputData = {10, 187, 225, 135};

        ModbusEquipment01.openConfig();

        ModbusEquipment01.setProperty( "Con_IPAddress", NewIP_InputData );

        ModbusEquipment01.commitConfig();


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: