How do you select the correct circuit breaker or fuse size for the ATV212 drives?
Issue:
Looking for a circuit breaker or fuse that is used with the ATV212 drive.

Product line:
Altivar 212

Environment:
All models, all serial numbers

Cause:
Recommended fuse rating for UL and CSA requirements.

Resolution:
The breaker and fuse sizing can be found in the ATV212 Quick Start Annex. The manual document is S1A7347602.

Schneider Electric Việt Nam

Phần đính kèm
ATV212 Annex.pdf [106.95 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: