Can the buttons on the faceplate of the ATV212 and ATV21 be disabled?
Issue:
Disable the keys on the faceplate of the ATV212 and ATV21.

Product line:
Altivar 21/212

Environment:
All models, all serial numbers

Cause:
How to disable the functionality of the buttons on the faceplate of the ATV21/212?

Resolution:
Press mode button to AUF
Press down arrow to F--- Press enter
Press down arrow to F730 (Up/down key reference) set to 1 (disable) press enter
Press down arrow to F732 (Loc/Rem key) set to 1 (disable) press enter
Press down arrow to F733 (Run/Stop key) set to 1 (disable) press enter
Press down arrow to F734 (Priority stop) set to 1 (disable) press enter
Press down arrow to F735 (HMI reset button) set to 1 (disable) press enter

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: