Can I transfer the program from an ATV56/ATV66/ATV16/ATV18/ATV28/ATV11 to any of our current drive products?

Issue:
Transfer configuration from an ATV56/ATV66/ATV16/ATV18 to any current drive product.

Product Line:
ATV56 Altivar ATV66 ATV18 ATV16 ATV28 ATV11

Environment:
All

Cause:
Replacement Drive

Resolution:
No.  You must manually program the new drive.
Most features and functions in the old drives can be found in the new ones, but some wiring changes may be required.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: