MiCOM blanking plates
Issue
Need blanking plates for a rack with MiCOM protection relays.

Product Line
MiCOM

Resolution
MiCOM Blanking Plate part numbers below:
  • GJ2028001                                 Blanking plate, MIDOS size 1 (Standard Grey)
  • GJ2028002                                 Blanking plate, MIDOS size 2, MiCOM size 10 TE (Standard Grey)
  • GJ2028003                                 Blanking plate, MIDOS size 3 (Standard Grey)
  • GJ2028004                                 Blanking plate, MIDOS size 4, MiCOM size 20 TE (Standard Grey)
  • GJ2028005                                 Blanking plate, MIDOS size 5 (Standard Grey)
  • GJ2028006                                 Blanking plate, MIDOS size 6, MiCOM size 30 TE (Standard Grey)
  • GJ2028007                                 Blanking plate, MIDOS size 7 (Standard Grey)
  • GJ2028008                                 Blanking plate, MIDOS size 8, MiCOM size 40 TE (Standard Grey)

Additional mounting screws (ZA0005094) can be ordered separately via the Transactional Sales Support group

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: