How long does the start/stop command have to be maintained in 3 wire control, to start and stop?

Issue:
Start/Stop configuration in a 3-wire control

Product Line:
ATS01

Environment:
All

Cause:
Timing effects on external devices.

Resolution:
==> In 3 wires, without deceleration, the stop command (S1) must be maintained at least 500ms and a pulse is enough for the start command (S2 - see attached file, page 5/7).
==> In 3 wires, with deceleration, a pulse is enough for the start / stop command (S2 & S1 - see attached file, page 6/7).

Schneider Electric Việt Nam

Phần đính kèm

ATS01 LT Instrucion Bulletint.pdfATS01 LT Instrucion Bulletint.pdf [1.04 MB]
Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: