What is the default username and password for ION/SPM/PME components?
Issue
What is the login credentials for ION/SPM/PME components

Product Line
ION Enterprise
StruxureWare Power Monitoring
Power Monitoring Expert

Environment
Schneider Electric Power Monitoring Software Applications

Cause
User may not know the default login credentials

Resolution
Note: At version 7.2 and later, there are no longer default user passwords for PME. During installation the password for supervisor user is configurable.

Enter one of the default username and passwords into required fields of each system component.

Username: supervisor
Password 0

or

Username: guest
Password: 0

The access level for the default usernames are:
Software VersionUsernameAccess Level
ION 5.xsupervisorSupervisor
ION 5.xguestSupervisor
ION 6.xsupervisorSupervisor
ION 6.xguestSupervisor
SPM 7.xsupervisorSupervisor
SPM 7.xguestObserver

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: