Are the Altivar ATV32/ATV320 Drives repairable?
Issue:
ATV32/ATV320 repairability

Product Line:
ATV32 ATV320

Environment:
All

Cause:
None

Resolution:
There are no repair parts for the ATV32/ATV320 drives, except for Heatsink Fan(s). However, if the drive is out of warranty, you can contact the repair depot at 1-800-950-9550 to see if they can repair it.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Danh mục:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi:
Danh mục: