NetBotz | Can I change the address on a NetBotz A-link sensor pod or rack access pod?
Issue:
Can I change the address on a NetBotz NBPD0150, NBPD0155, or NBPD0170?

Product Line:
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)
NetBotz Sensor Pods (NBPD0150 & NBPD0155)
NetBotz Rack Access Pod (NBPD0170)

Environment:
NetBotz (all versions)

Cause:
NetBotz A-link sensor pods and rack access pods get their addresses programmatically.

Resolution:

There is no way to manually configure the address on these pods.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: