How do I activate / deactivate PID function on the ATV32 Series drives?
Issue:
ATV32 PID function activate / deactivate

Product Line:
Altivar 32 series drives.

Environment:
All models, All serial numbers.

Cause:
Need to activate or deactivate PID function on ATV32 series drive.

Resolution:
Navigate to the PIF parameter via the following menus:  DRI -> Conf -> Full -> Fun -> PID-

PIF parameter assigns the PID feedback to a specific input terminal. To deactivate PID (deactivated by default) set this parameter to NO.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: