The A and B states of the Quantum Hot Standby CPU's are established based upon MAC address. The lowest MAC address will by default become the "A" CPU. Is it possible to change this behavior?


Yes. During commissioning you can assign the CPU with the higher MAC address to "A" .

1: Power up the CPU with the higher MAC address.
2: Using the keypad on the CPU assign the "A" attribute to the CPU.
3: Download the application to the PLC and issue a start command.
4: Power up the Standby while holding down the ESC key on the keypad.
5: When the screen displays "Erasing All RAM wait 2 seconds" let go of the ESC key.
6: The CPU should become Standby and take on the "B" attribute.



R-82917

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: