What should parameter bFr be set to if you are using a 50hz 400vac motor?

Issue:
Setting up bFr parameter for a 50hz 400vac motor.

Product Line:
ALTIVAR ATV61

Environment:
All

Cause:
Installation / Setup

Resolution:
Drive settings for bFr, nPr, UnS , nCr and nSP settings,  should match the motor nameplate.
in this case bFr will be set to 50hz and UnS will be set to 400vac

Schneider Electric Việt Nam

Phần đính kèm

atv61_programming_manual_en_1760649_08.pdfatv61_programming_manual_en_1760649_08.pdf [4.35 MB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: