What are the part numbers of the terminal block for the BMXAMI0800?
Issue:
What are the part numbers of the terminal block for the BMXAMI0800?

Product Line:
X80 I/O Modules

Resolution:
There are 2 types of terminal blocks for the BMXAMI0800.  Cage clamp-type part number BMXFTB2800 or Spring-type part number BMXFTB2820.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: