Configuring GOOSE in MiCOM S1 Studio
Issue
The process of setting up basic GOOSE messaging between two MiCOM Px40 relays within MiCOM S1 Studio is not described in the User Manuals.

Product Line
MiCOM Px4x IEDs with Version 2 implementation of IEC 61850

Environment
MiCOM S1 Studio V3.5.1 and up

Resolution
Refer to attached Tutorial which describes the procedure for configuring GOOSE messaging: 'Configuring GOOSE in MS1S - 988-1187327_CA_WEB.pdf'

Schneider Electric Việt Nam

Phần đính kèm
Configuring GOOSE in MS1S - 998-1187327_CA_WEB.pdf [2.08 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: