What drives will the VW3A8120 simple loader tool work with?

ATV31 -        V1.1 IE01 or higher
ATV312 -      V1.3 IE01 or higher
ATV71 -        V1.1 IE01 or higher
ATV71 S383  V1.1 IE01 or higher
ATV71 Lift -   V1.1 IE01 or higher
ATV61 -        V1.1 IE01 or higher
ATV12 -        V1.3 IE01 or higher
ATV32 -        V1.5 IE01 or higher
ATV320 -      V2.7IE23 or higher

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Phần đính kèm
Simple-Loader_IS_AAV50335_03.pdf [625.89 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: