Using Symmetra RM outside of a Rack (Symmetra RM Floor Mounting Kit)
Issue:
I do not want to mount Symmetra RM in a rack; I want to put it on the floor.  What are my options?

Product Line:
Symmetra RM

Environment:
All serial ranges

Cause / Overview:
Some applications require that a Symmetra RM UPS not be mounted in a rack.  This article details the options that are currently available to the customer.

Resolution:
There is an optional floor mount kit available for the Symmetra RM UPS, SYOPT1.  This can be used to install the UPS chassis in a tower configuration and is the only approved method to do so.  More information can be found at the following links:

SYOPT1 Product Page - http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=SYOPT1&tab=models
SYOPT1 Install Manual - hhttps://www.apc.com/us/en/download/document/SPD_ASTE-6Z8LMU_EN/

Please Note: The SYOPT2, SYOPT10, and SYOPT11 that are mentioned in the guide have been DISCONTINUED and are no longer available.  The SYOPT1 is the only piece of the floor mount kit currently available.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: