ATV61 and ATV71 VW3A1101 remote keypad does not allow any selections to be made when pushing the enter button.
Issue:
ATV61 and ATV71 VW3A1101 remote keypad does not allow any selections to be made when pushing the enter button.

Product Line:
Altivar ATV61 and ATV71 VW3A1101

Environment:
All

Cause:
Enter button does not appear to work.

Resolution:
Make sure the drive is not running first.
Try swapping out the HMI keypads
Check to see if the buttons on the face of the drive work.
Try mounting the remote HMI on the face of the drive to see if the enter button works.
Try swapping out the cables.
Try using the modbus Canopen port vs the hmi port.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: