Can the ATV312 Drive switch from local keypad control to remote terminal control by pressing and holding the mode button?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
ATV312, local mode to remote mode.

Product:
ATV312  Altivar 312

Environment:
All

Cause:
Programming was changed.

Resolution:
The drive can be changed from remote (Terminal) mode to local (Keypad) mode by pressing and holding the mode for 3 seconds.
However, when returning to remote from local requires the drive to be reset to factory defaults using the FCS parameter in the drC menu.
Consult the ATV312 Programming manual for details.
https://www.se.com/ww/en/download/document/BBV46385/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: