Unity Pro error message 'Project is read only'.
Issue:
Error message is displayed when trying to open a Unity Pro project.

Product Line:
Unity Pro programming software

Resolution:
-  Is the project open in another session of Unity?
-  Go to the Windows Explorer. Right click on the project file and verify that the 'read only ‘ attribute is not set.
-  Is the Unityxl.ini file attribute set for ‘read only’?
-  Go to Tools – Options – Connection. Make sure that programming mode is set.
-  File - Open.  Make sure that 'read only mode' is not checked in the 'Open Options' in the lower left corner of the Open box.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: